OBO resorts the rail system
Practical selection aid and new structures provide greater clarity
For many years, electricians around the world have put their faith in the trusted rail system from OBO Bettermann. To make ordering and installation even easier, OBO has resorted the product range. It is now easy to choose the right product at a glance from the three load classes: Light-duty, medium-duty and heavy-duty. The accessories are also right there in the selection aids of the appropriate rail types.
The robust rail systems are used together with countless other OBO products around the world. For example, they are used as a key component in the suspended construction of cable tray systems, as fastening rails for clamp clips for cable routing or as mounting rails.
Besides the three load classes, light-duty, medium-duty and heavy-duty, the rails are also available to electrical installation engineers in various material thicknesses. A comprehensive range of hole patterns, always matching the appropriate application, rounds off the portfolio. A further advantage: Depending on the use location, the rail range is available with the two surfaces, strip galvanised and hot-dip galvanised, and in the stainless steel qualities A2 and A4.
With the practical selection aid, the user can rapidly obtain an overview of the different variants, accessories parts and combination options. Thus, there is nothing in the way of the correct selection.