Solutions for the nacelle of wind power plants
The nacelle is located in the tower of the wind power plant. The two components are connected via a rotating joint. The rotor, consisting of the hub and individual rotor blades, is located at the front of the nacelle. The nacelle transfers the loads resulting from the rotor and all installed components to the foundation via the tower.
The wind turbine nacelle is often referred to as the powerhouse, as it is the core of the wind power plant. Inside are some of the most important components of the plant, such as the generator for producing electricity. However, the highest vibrations and oscillations occur in the area of the nacelle and the tower head. This means that the installation systems installed there are also subject to special requirements. OBO offers the maximum safety in this area with protection solutions for the wind turbine nacelle.

OBO system solutions for wind turbine nacelles
- Surge arrester V20 with a total discharge capacity of 60 kA (20/40 kA / pole)
- Surge protection for high-speed networks up to 1 GB with data line protection devices for high-speed networks up to 1 GB
- GR-Magic® mesh cable tray with the patented, plug-in connection system
- Wall and support bracket for screwless mesh cable tray fastening
- Robust junction boxes for safe IP protection of electrical cabling
- Magnetic card and holder for recording pulsed and lightning currents
- Insulated air-termination rod for inner-routed isCon conductors with side exit: explaining the isCon system